MW.FAULTS
Any time a MechaWare fault is issued additional details will be available in MW.FAULTS. The most likely causes are misconfiguration of a block or keyword, or something in a custom MechaWare model.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-12-00-000 |
General Information
| Type | Read Only |
| Description | Retrieve verbose warning information about MechaWare related faults |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | String |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.